Using OpenSDA in a Custom Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using OpenSDA in a Custom Board

1,798件の閲覧回数
gustavocosta
Contributor III

Hi there,

I'm moving to my custom board now and my initial idea was to use the OpenSDA circuitry in it to provide an easy way of flashing and debug my K64 MCU. 

The MCU I choose to work with was MK64FN1M0VLQ12 so it is a different package compared to the ones present in FRDM-K64 and TWR-K64.

My question is: Will I be able to use this circuit for flashing, debugging and communicate (USB to Serial) considering those differences?

Also, should I use the OpenSDA circuitry based on FRDM or TWR?

Thank you very much.

Best regards,

Gustavo Costa

R&D Engineer

ラベル(3)
0 件の賞賛
返信
1 返信

1,639件の閲覧回数
javierhernande1
Contributor IV

Hi,

You can use USB DFU if you want that the user can update the firmware trought a pc.  USB DFU boot loader for MCUs 

With KSDK and uTasker is possible.  µTasker USB Device Configuration 

You can use SWD o JTAG to debug.

OpenSDA is not recommended to production.

Best regards

0 件の賞賛
返信