Using OpenSDA in a Custom Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using OpenSDA in a Custom Board

1,740 次查看
gustavocosta
Contributor III

Hi there,

I'm moving to my custom board now and my initial idea was to use the OpenSDA circuitry in it to provide an easy way of flashing and debug my K64 MCU. 

The MCU I choose to work with was MK64FN1M0VLQ12 so it is a different package compared to the ones present in FRDM-K64 and TWR-K64.

My question is: Will I be able to use this circuit for flashing, debugging and communicate (USB to Serial) considering those differences?

Also, should I use the OpenSDA circuitry based on FRDM or TWR?

Thank you very much.

Best regards,

Gustavo Costa

R&D Engineer

0 项奖励
回复
1 回复

1,581 次查看
javierhernande1
Contributor IV

Hi,

You can use USB DFU if you want that the user can update the firmware trought a pc.  USB DFU boot loader for MCUs 

With KSDK and uTasker is possible.  µTasker USB Device Configuration 

You can use SWD o JTAG to debug.

OpenSDA is not recommended to production.

Best regards

0 项奖励
回复