Using OCRAM on MKV58F1M0xxx24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using OCRAM on MKV58F1M0xxx24

Jump to solution
2,553 Views
lsrbigfoot
Contributor IV

Hello,

I am looking to utilize the 64KB OCRAM (Range 0x2F000000 - 0x2F00FFFF) on the MKV58F1M0VLQ24 like regular SRAM for basic read/write of data.

Where can I find code examples (driver examples) that utilize the OCRAM?

What prerequisites (initialization) must be done before OCRAM can be accessed?

Thanks!

Tags (1)
0 Kudos
Reply
1 Solution
2,395 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Leighton Rowe,

 

There are no initializations needed in order to use the OCRAM. This can be accessed as the regular SRAM.

 

You can take the following document as reference to relocate data and code in the OCRAM.

 

https://community.nxp.com/docs/DOC-335283

 

I hope this helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
2,396 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Leighton Rowe,

 

There are no initializations needed in order to use the OCRAM. This can be accessed as the regular SRAM.

 

You can take the following document as reference to relocate data and code in the OCRAM.

 

https://community.nxp.com/docs/DOC-335283

 

I hope this helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------