Using OCRAM on MKV58F1M0xxx24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using OCRAM on MKV58F1M0xxx24

ソリューションへジャンプ
2,588件の閲覧回数
lsrbigfoot
Contributor IV

Hello,

I am looking to utilize the 64KB OCRAM (Range 0x2F000000 - 0x2F00FFFF) on the MKV58F1M0VLQ24 like regular SRAM for basic read/write of data.

Where can I find code examples (driver examples) that utilize the OCRAM?

What prerequisites (initialization) must be done before OCRAM can be accessed?

Thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
2,430件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Leighton Rowe,

 

There are no initializations needed in order to use the OCRAM. This can be accessed as the regular SRAM.

 

You can take the following document as reference to relocate data and code in the OCRAM.

 

https://community.nxp.com/docs/DOC-335283

 

I hope this helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,431件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Leighton Rowe,

 

There are no initializations needed in order to use the OCRAM. This can be accessed as the regular SRAM.

 

You can take the following document as reference to relocate data and code in the OCRAM.

 

https://community.nxp.com/docs/DOC-335283

 

I hope this helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------