Using NXP(Freescale) VID and PID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using NXP(Freescale) VID and PID

ソリューションへジャンプ
2,145件の閲覧回数
evgenik
Contributor IV

Hello.

I am developing my commercial product that will have a USB-CDC communication protocol. I do not want to pay $5000 for my identifier. According to this, I have several questions:

  1. Can I use Freescale's VID 0x2504 and PID 0x0300 in my commercial product without buying my own?
  2. Can I leave Freescale's VID 0x2504 and PID 0x0300 identifiers, and change only the string descriptor with "Freescale semiconductor inc." to my personal or do I need to leave everything unchanged?
  3. Is using Freescale VID 0x2504 and PID 0x0300 in my commercial product a trademark infringement or something like that?

Thanks.

ラベル(1)
  • USB

0 件の賞賛
返信
1 解決策
2,009件の閲覧回数
mjbcswitzerland
Specialist V

Hi

See Application To Use NXP's USB-IF Vendor ID (mid-2019) | NXP Semiconductors 

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,010件の閲覧回数
mjbcswitzerland
Specialist V

Hi

See Application To Use NXP's USB-IF Vendor ID (mid-2019) | NXP Semiconductors 

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

0 件の賞賛
返信