Using NXP(Freescale) VID and PID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using NXP(Freescale) VID and PID

Jump to solution
2,205 Views
evgenik
Contributor IV

Hello.

I am developing my commercial product that will have a USB-CDC communication protocol. I do not want to pay $5000 for my identifier. According to this, I have several questions:

  1. Can I use Freescale's VID 0x2504 and PID 0x0300 in my commercial product without buying my own?
  2. Can I leave Freescale's VID 0x2504 and PID 0x0300 identifiers, and change only the string descriptor with "Freescale semiconductor inc." to my personal or do I need to leave everything unchanged?
  3. Is using Freescale VID 0x2504 and PID 0x0300 in my commercial product a trademark infringement or something like that?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,069 Views
mjbcswitzerland
Specialist V

Hi

See Application To Use NXP's USB-IF Vendor ID (mid-2019) | NXP Semiconductors 

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

View solution in original post

0 Kudos
Reply
1 Reply
2,070 Views
mjbcswitzerland
Specialist V

Hi

See Application To Use NXP's USB-IF Vendor ID (mid-2019) | NXP Semiconductors 

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

0 Kudos
Reply