Using Multiple LPUARTS in different Ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Multiple LPUARTS in different Ports

ソリューションへジャンプ
1,711件の閲覧回数
CEPL_Dev
Contributor III

Microcontroller - NXP Kinetis MKE14F512VLL16

IDE - MCUXpresso v11.3.0

SDK - SDK_2.x_MKE14F512XXX16 ,v2.8.8

Hello,

I've an application in which I have to use the same LPUART module in two different ports. Different peripheral is connected to each port and I don't want to use them simultaneously.

Peripheral 1(P1) is connected to:

PTA3 (ALT6)- LPUART0-TX

PTA2 (ALT6)- LPUART0-RX

 

Peripheral 2(P2) is connected to:

PTB0 (ALT2)- LPUART0-RX

PTB1 (ALT2)- LPUART0-TX

In my application, I'm initializing the LPUART0 module with Port A2 and A3 using the following code.

 

 

void InitLPUART0(void){
PCC->CLKCFG[PCC_LPUART0_INDEX] |= PCC_CLKCFG_PCS(3); //System Oscillator Bus Clock
PCC->CLKCFG[PCC_LPUART0_INDEX] |= PCC_CLKCFG_CGC(1); //PCC Configuration - Enable Clock

PORTA->PCR[2] |= PORT_PCR_MUX(6); /* LPUART - ALT6 */
PORTA->PCR[3] |= PORT_PCR_MUX(6);

LPUART0->CTRL &= ~(LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);
LPUART0->BAUD = BAUD_115200; //48M/(26*16)Baud rate for 115200bps

LPUART0->CTRL |= LPUART_CTRL_RIE(1); /* Receiver Interrupt Enable */
LPUART0->CTRL |= LPUART_CTRL_TE(1); /* Transmitter enable */
LPUART0->CTRL |= LPUART_CTRL_RE(1); /* Receiver Enable */

NVIC_EnableIRQ(LPUART0_RX_IRQn); 
}

 

 

 

Initially ,this is working as expected. The system is sending data as expected through the port.

When I need to use the other peripheral, I'm shifting the LPUART0 to the other port as shown below.

 

 

LPUART0->CTRL &= ~(LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK); /* Disable Tranceiver */

PORTA->PCR[3] |= PORT_PCR_MUX(1); /* LPUART - ALT1 - GPIO */
PORTA->PCR[2] |= PORT_PCR_MUX(1);

PORTB->PCR[0] |= PORT_PCR_MUX(2); /* LPUART - ALT2 - UART */
PORTB->PCR[1] |= PORT_PCR_MUX(2);

LPUART0->CTRL |= (LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK); /* Enable Tranceiver */

 

 

 

After shifting the system is supposed to send the data through the Port B to peripheral 2. But the LPUART lines are idle even though the transmission code is running. After switching ports, if I switch back to peripheral 1 in Port A using the same method, it doesn't respond either.

The system is working if use either of the ports without switching to the another.

What is wrong in this method?

Regards
Prasanth
0 件の賞賛
返信
1 解決策
1,704件の閲覧回数
CEPL_Dev
Contributor III

Hello all,

Just found out the solution. I was overwriting bits 8, 9 and 10 corresponding to the MUX settings in the PORTx_PCR register instead of clearing them. 

Corrected method is posted below.

 

 

void SelectCOMPort(COMPORT_TYPE CPort){ /* Directs LPUART0 to the required port and disables others */
	LPUART0->CTRL &= ~(LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);	/* Disable Tranceiver */
	switch (CPort)
	{
	case PORT_1:
		PORTB->PCR[0] &= ~(BIT8 | BIT9 | BIT10); 	/* LPUART - Disable */
		PORTB->PCR[1] &= ~(BIT8 | BIT9 | BIT10);

		PORTA->PCR[3] |= PORT_PCR_MUX(6); 			/* LPUART - ALT6 - to UART */
		PORTA->PCR[2] |= PORT_PCR_MUX(6);

		break;
	case PORT_2:
		PORTA->PCR[3] &= ~(BIT8 | BIT9 | BIT10);  	/* LPUART - Disable */
		PORTA->PCR[2] &= ~(BIT8 | BIT9 | BIT10);

		PORTB->PCR[0] |= PORT_PCR_MUX(2); 			/* LPUART - ALT2 - to UART */
		PORTB->PCR[1] |= PORT_PCR_MUX(2);
		break;
	default:
		break;
	}
	LPUART0->CTRL |= (LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);	/* Enable Tranceiver */
}

 

 

 

Regards
Prasanth

元の投稿で解決策を見る

1 返信
1,705件の閲覧回数
CEPL_Dev
Contributor III

Hello all,

Just found out the solution. I was overwriting bits 8, 9 and 10 corresponding to the MUX settings in the PORTx_PCR register instead of clearing them. 

Corrected method is posted below.

 

 

void SelectCOMPort(COMPORT_TYPE CPort){ /* Directs LPUART0 to the required port and disables others */
	LPUART0->CTRL &= ~(LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);	/* Disable Tranceiver */
	switch (CPort)
	{
	case PORT_1:
		PORTB->PCR[0] &= ~(BIT8 | BIT9 | BIT10); 	/* LPUART - Disable */
		PORTB->PCR[1] &= ~(BIT8 | BIT9 | BIT10);

		PORTA->PCR[3] |= PORT_PCR_MUX(6); 			/* LPUART - ALT6 - to UART */
		PORTA->PCR[2] |= PORT_PCR_MUX(6);

		break;
	case PORT_2:
		PORTA->PCR[3] &= ~(BIT8 | BIT9 | BIT10);  	/* LPUART - Disable */
		PORTA->PCR[2] &= ~(BIT8 | BIT9 | BIT10);

		PORTB->PCR[0] |= PORT_PCR_MUX(2); 			/* LPUART - ALT2 - to UART */
		PORTB->PCR[1] |= PORT_PCR_MUX(2);
		break;
	default:
		break;
	}
	LPUART0->CTRL |= (LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);	/* Enable Tranceiver */
}

 

 

 

Regards
Prasanth