Using FTM3 with Internal Oscillator (KV31f512)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using FTM3 with Internal Oscillator (KV31f512)

1,298 Views
p_hedlund
Contributor II

I am using the internal oscillator with the KV31F512 Processor.

Our application is a Brushless DC motor controller. (phase u Hi, low, phase v hi, low and phase w hi and low)

I was given a board design that already existed but was never tested.

All 3 of the lo phases are just on and off, All 3 of the hi phases are gated PWM's 

Phase U is PortA13 FTM1-CH1

Phase V is PortE25 FTM0-CH1

Phase W is PortE6  FTM3-CH1

Using the FRDM-kv31f and subbing PortC2 for PortE25 The software runs and i get the expected signals.

Our Target board however does not an external crystal and we must use the internal oscillator.

I have an UART2 working at 115200 without issue.

I have a timer running to control the start/stop of the 3 phases.

PhaseW does not work.

Further testing has found that if i comment out code for Phase U and Phase V, and only have Phase W enabled, I get pulses on Phase U.

Since this worked on the FRDM-KV31F board and not our target I am wondering if there is some interaction i am unaware of when using the internal oscillator.

If you need to I can send code snippets to show what i am doing.

I know the preferred method is to use ONE FTM for a motor but the layout was already done.

Thanks in advance.

Peter Hedlund

0 Kudos
Reply
1 Reply

1,264 Views
p_hedlund
Contributor II

Problem Fixed - When timer was enabled was the issue.

0 Kudos
Reply