Use FRDM-KL25Z as a debug probe.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use FRDM-KL25Z as a debug probe.

跳至解决方案
4,868 次查看
jun1
Contributor V

Thank you for your help.

It cut J11 as shown in the FRDM-KL25Z user's manual and connected to SWDCLK and SWDDIO of the MCU outside the board.
The external MCU is MKM14Z64ACHH5.

If you set the debugger to PE-micro from EWARM of IAR and write to flash
First, when the PEMICRO Connection Manager screen appears and press Connect, an error message appears.

Error 17926. Target Type MCU mismatch. Unexpected processor detected. Aborting debug sesion.

① Does OpenSDA of FRDM-KL25Z check the CPU, and an MCU different from the KL25Z in the board causes an error?
② Is there a way to avoid this error and erase / write the external MKM14Z64ACHH5?


Thanks for your instruction.

0 项奖励
回复
1 解答
4,566 次查看
BlackNight
NXP Employee
NXP Employee

If using the P&E default firmware, you only can program a microcontroller of the same type, see Using the Freedom Board as SWD Programmer | MCU on Eclipse 

An option would be to use USBDM, see Debug External Processors with USBDM and Freedom Board | MCU on Eclipse , or see here more on this topic: Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,567 次查看
BlackNight
NXP Employee
NXP Employee

If using the P&E default firmware, you only can program a microcontroller of the same type, see Using the Freedom Board as SWD Programmer | MCU on Eclipse 

An option would be to use USBDM, see Debug External Processors with USBDM and Freedom Board | MCU on Eclipse , or see here more on this topic: Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

I hope this helps,

Erich

0 项奖励
回复
4,566 次查看
jun1
Contributor V

Thank you very much.
understood.

jun

0 项奖励
回复