Use FRDM-KL25Z as a debug probe.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use FRDM-KL25Z as a debug probe.

ソリューションへジャンプ
4,776件の閲覧回数
jun1
Contributor V

Thank you for your help.

It cut J11 as shown in the FRDM-KL25Z user's manual and connected to SWDCLK and SWDDIO of the MCU outside the board.
The external MCU is MKM14Z64ACHH5.

If you set the debugger to PE-micro from EWARM of IAR and write to flash
First, when the PEMICRO Connection Manager screen appears and press Connect, an error message appears.

Error 17926. Target Type MCU mismatch. Unexpected processor detected. Aborting debug sesion.

① Does OpenSDA of FRDM-KL25Z check the CPU, and an MCU different from the KL25Z in the board causes an error?
② Is there a way to avoid this error and erase / write the external MKM14Z64ACHH5?


Thanks for your instruction.

ラベル(2)
0 件の賞賛
返信
1 解決策
4,474件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If using the P&E default firmware, you only can program a microcontroller of the same type, see Using the Freedom Board as SWD Programmer | MCU on Eclipse 

An option would be to use USBDM, see Debug External Processors with USBDM and Freedom Board | MCU on Eclipse , or see here more on this topic: Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,475件の閲覧回数
BlackNight
NXP Employee
NXP Employee

If using the P&E default firmware, you only can program a microcontroller of the same type, see Using the Freedom Board as SWD Programmer | MCU on Eclipse 

An option would be to use USBDM, see Debug External Processors with USBDM and Freedom Board | MCU on Eclipse , or see here more on this topic: Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信
4,474件の閲覧回数
jun1
Contributor V

Thank you very much.
understood.

jun

0 件の賞賛
返信