Understanding the Kinetis HEX file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Understanding the Kinetis HEX file

ソリューションへジャンプ
2,190件の閲覧回数
sfarzan
Contributor I

Hi everybody,

I'm trying to understand the hex file created by CodeWarrior for KL16. The hex file has the following structure:

:10000000000C00206D31000025310000253100007A

:1000100000000000000000000000000000000000E0

:10002000000000000000000000000000253100007A

:100030000000000000000000253100002531000014

:100040002531000025310000253100002531000058

:10005000000000002531000025310000253100009E

:100060002531000025310000253100002531000038

...

:106C3000306C000000FCFF1F00000000000000009E

:086C400000000000000000004C

:040000030000316D5B

:00000001FF

I know that second and third bytes show the address following by 1 byte (?) and then 16 bytes of code and finally another extra byte (?).

It seems the last three lines don't have this structure. Could you please tell me what these three lines refer to?

Thanks in advance.


ラベル(1)
0 件の賞賛
返信
1 解決策
1,964件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
1 返信
1,965件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信