Unable to unsecure MKL26Z64VFT4 and reset signal issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to unsecure MKL26Z64VFT4 and reset signal issue

1,373 Views
dileeptn
Contributor I

hai,

we are using the MKL26z64ft4 in our latest project. We are presently using samples which were provided as per our request from the NXP. When i try to program it using somany IDE and compilers it shows error that could not be "erased and connection to target failed. The mcu which is flash locked. so i need to unlock it to use for my projects. But till icant, i tried Keil, CodeWarrier and the Kinetis design studio also but i am failed to debug the MCU. Anyone still facing issues like this? I cant even access my target MCU but the ic address is visible in keil using ulink only not for jlink. in jlink it doesnt detect the mcu id.Could you please suggest the possible reasons which could lead to the error  How should we move forward with the debugging of the IC.Please suggest us the steps and procedures to be followed to overcome this issue while debugging the board.Is there any hardware wise setup which we should check whether we have implemented in our design which could have lead to such an error? Am looking forward to hear from you.....................

I am facing a issue in our board that the reset pin which gives an pulse waveform not a permanent high or low. Is that the issue for not accessing the chip? But the vpp for the reset which is 3.3v. I am confused. The reset is pulled upwith 10k and a switch connected to it from ground. if the switch is pressed the reset goes low but when i released the switch the pulse came. any one faced issue like this?What is your suggestion regarding the issue?

Any help will be appreciated.

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,274 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Customer,

    This is the same question as your another post, please check that post, I already reply you:

Unable to unlock MKL26z64vft4 

 


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply