Unable to load or delete MK20DX256VLL10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to load or delete MK20DX256VLL10

3,759件の閲覧回数
VasaPon
Contributor I

Hi,

we are using MK20DX256VLL10 processor. On some boards with the same software, the processor stops working. It is not yet clear to me why. Will it go to a state where it is not possible to upload or delete, could anyone advise? Attached sends a log extract from J-Link. I also looked at the reset pin with the oscilloscope and there is a 66us period on it. Is the processor destroyed or can it still be played?

Thank you in advance for your reply.

0 件の賞賛
返信
3 返答(返信)

3,724件の閲覧回数
VasaPon
Contributor I

Thank you very much, in the end I managed to delete the processor and load it in CodeWarior -> Erase and flash program. He also deleted all the flash banks and uploaded the bin file, but when reading the Flash memory the result is a completely different part of the memory was not loaded. From this I conclude that the processor is damaged.
I will definitely look at your progress.

Does anyone know what could damage Flash?

0 件の賞賛
返信

3,718件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Flash could not be damaged easily, even cycling over 50k times. But of course some abnormal use case may damage the chip, like the document says, welding problem or power issue.

 

Regards,

Jing

0 件の賞賛
返信

3,740件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @VasaPon ,

You said there is period reset signal on RESET pin. Please refer to this file. You may have same problem.

 

Regards,

Jing

0 件の賞賛
返信