Unable to flash target microcontroller anymore

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to flash target microcontroller anymore

1,611件の閲覧回数
melvinroopith
Contributor I

Hi,

I was able to flash the target microcontroller (MKL05Z32VLF4) for a few times via the SWD interface without any problem, but later on after a few times the flashing was not happening. Upon measuring the voltage difference between the reset pin and ground, it was 1.8V, while the resistance between the reset pin and ground showed 3K ohms. I cross-checked the voltage difference and resistance at the reset pin with another identical target microcontroller, and i got the readings as 3.2V and 8K ohm respective. What could be the possible reasons that the reset pin voltage and resistance are altered over the usage?

Any form of suggestion / input will be appreciated. Thanks in advance.
- Melvin

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,475件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Melvin,

There with some threads might with the same issue as yours board.

Please check below links for the detailed info:

Problem to program KL05Z - reset_b oscillation

KL05 reset line problem?

Kinetis KL05 SWD Connectivity Problems


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信