Unable to Debug FRDM-KL28Z board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Debug FRDM-KL28Z board

1,133件の閲覧回数
talledo
Contributor I

Hi

While I can debug OK with a different PC. I have a fresh MCUXpresso installed on a different PC. I connect my FRDM-KL28Z board but I am not able to debug. I get the following:

MCUXpresso IDE RedlinkMulti Driver v11.1 (Feb 24 2020 13:54:38 - crt_emu_cm_redlink build 11)
Found part description in XML file MKL28Z7_internal.xml
Reconnected to existing LinkServer process.
============= SCRIPT: kinetisconnect.scp =============
Kinetis Connect Script
Connecting to Probe Index = 1
This probe = 1
This TAP = 0
This core = 0
DpID = 2BA01477
Assert NRESET
Reset pin state: 00
Error: Wire Ack Wait Fault
Power up Debug
Error: Wire Ack Wait Fault
Error: Wire Ack Wait Fault
Error: Wire Ack Wait Fault
MDM-AP APID: 0xF0000F00
MDP-AP Not Found
============= END SCRIPT =============================
Probe Firmware: DAPLink CMSIS-DAP (ARM)
Serial Number: 0205000033514e4500105015846c00366cb1000097969900
VID:PID: 0D28:0204
USB Path: \\?\hid#vid_0d28&pid_0204&mi_03#7&1fb670f8&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
connection failed - Em(01). Cannot find MEM-AP selected by core index (check target power).. Retrying
Failed on connect: Em(01). Cannot find MEM-AP selected by core index (check target power)
Connected&Reset. Was: NotConnected. DpID: 2BA01477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 0
No debug bus (MemAp) selected
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.

The difference when I connect to the non working PC. Windows 10 shows a mbed Serial Port  while when I connect to the good PC, that driver is not shown when I connect the FRDM-KL28z board.

Any suggestions?

0 件の賞賛
返信
1 返信

1,083件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

1.Check your Dap driver on computer .

2.Check your signature on computer

3.update your opensda

You can check and troubleshoot according above options.

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信