USB3.0 and K65

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,979件の閲覧回数
goranigic
Contributor II

I am using K65, external SDRAM, and SD card. Is it possible to connect FT600 to that configuration?

I know that FT600 doesn't have FLEX-BUS. I am also using K65 USB 2.0 port.

This is the last moment customer request to add USB3.0 support (as second USB port).

Thanks,

g

p.s.

I have seen the discussion:

usb3.0 with K80

ラベル(3)
0 件の賞賛
返信
1 解決策
2,758件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

K65 product has the Flexbus module.

The chapter 34 of K65 reference manual provides the detailed info.

There is an application note about multiplexing pins between SDRAM and Flexbus on K65.

For more detailed info, please check here.


Wish it helps
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,758件の閲覧回数
goranigic
Contributor II

K65 doesn't have FLEXBUS
FT600 uses 16b FIFO

Thanks,

g

0 件の賞賛
返信
2,759件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

K65 product has the Flexbus module.

The chapter 34 of K65 reference manual provides the detailed info.

There is an application note about multiplexing pins between SDRAM and Flexbus on K65.

For more detailed info, please check here.


Wish it helps
Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,758件の閲覧回数
goranigic
Contributor II

Thanks,

It doesn't have flex memory, but it has the flex bus.

I appreciate your response

g

0 件の賞賛
返信