USB voltage regulator problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB voltage regulator problem

ソリューションへジャンプ
3,171件の閲覧回数
jimclay
Contributor II

IN a custom design using the Kinetis K61 we have a directly connected USB interface (no ULPI), running in full-speed mode as a usb device, not host. It has protection diodes commonly used for a usb device connection on the D+ and D- lines. While testing our usb stack we connect and reconnect the cable multiple times. During this process we have managed to kill the interface on two boards in just a few days. The internal regulator seems to be shot as it only produces about a half volt from the 5V supplied. Static precautions are taken. The device descriptors are set to bus powered mode, no current requested.

Has this problem been seen before?  What can we do to fix and/or prevent this?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,767件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello Jim,

    

Did you add series ferrites on VBUS and GDN pins from USB port? You could refer to the USB connection of a Freescale Board (Freedom) which is also Bus powered; on this board, the GND and VBUS signals from USB port are connected to ferrites, but they have internal resistance of 330 ohm. You can review these details on Freedom´s schematic, available at the following link:

www.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf

    

Hope this information will be useful for you.

Best regards!

/Carlos.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,767件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello Jim,

    

Did you add series ferrites on VBUS and GDN pins from USB port? You could refer to the USB connection of a Freescale Board (Freedom) which is also Bus powered; on this board, the GND and VBUS signals from USB port are connected to ferrites, but they have internal resistance of 330 ohm. You can review these details on Freedom´s schematic, available at the following link:

www.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf

    

Hope this information will be useful for you.

Best regards!

/Carlos.

0 件の賞賛
返信
2,767件の閲覧回数
jimclay
Contributor II

No, we did not have the series ferrites.  Thanks for the tip.

0 件の賞賛
返信