USB min frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB min frequency

跳至解决方案
1,780 次查看
martindusek
Contributor V

Hello,

what's the min CPU frequency Freesscale bare metal USB stack (namely generic HID device) can reliably run on KL26?

I clock USB module 48 MHz.

When I compile my C code without optimization and CPU runs on 12 MHz I mainly get "USB device not recognized" error in Windows when I connect my device to PC (90% probability I will get the error)

No optimization and 24 Mhz CPU leads to "USB device cannot start, Code 10" in Windows (10 % probabality I will get the error)

Optimization and 12 MHz CPU leads to "USB device cannot start, Code 10" in Windows (10 % probabality I will get the error)

Optimization and 24 Mhz leads to no error.

标签 (1)
0 项奖励
回复
1 解答
1,646 次查看
mjbcswitzerland
Specialist V

Hi

pastedImage_0.png

When I run the uTasker USB-HID mouse on the FRDM-KL26Z I can set the system clock to 24MHz and the Flash/Bus clocks to 3MHz and build with GCC with no optimisation and it operates normally (connected >20 times without any errors). Generally there shouldn't be much time critical with the enumeration process.

Regards

Mark

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,647 次查看
mjbcswitzerland
Specialist V

Hi

pastedImage_0.png

When I run the uTasker USB-HID mouse on the FRDM-KL26Z I can set the system clock to 24MHz and the Flash/Bus clocks to 3MHz and build with GCC with no optimisation and it operates normally (connected >20 times without any errors). Generally there shouldn't be much time critical with the enumeration process.

Regards

Mark

0 项奖励
回复