USB bootloader for MK60 MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB bootloader for MK60 MCU

2,701件の閲覧回数
rabbit
Contributor III

I am looking for USB bootloader for MK60 MCU,  any suggestions will be appreciated.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,225件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Please kindly refer to the following links for details.

USB Mass Storage Device Host Bootloader:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4368.pdf?fsrch=1&sr=1

USB DFU Bootloader:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf?fsrch=1&sr=1

Hope that helps,

B.R

Kan

0 件の賞賛
返信

2,225件の閲覧回数
rabbit
Contributor III

Our board is using MK60N512.

For this bootloader via USB, is it boot from USB driver or from PC USB port?

0 件の賞賛
返信

2,225件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

These two bootloaders are both accepted bin file sent from PC USB port, the main difference is DFU bootloader needs a GUI PC tool to download the file while USB Mass Storage Device Host Bootloader needn't.

Hope that helps,

B.R

Kan

0 件の賞賛
返信