USB VBUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB VBUS

6,065件の閲覧回数
a8Chcx
Contributor V

Hi,

I am using K66F MCU to build USB HID to communicate with PC. And I have the problem:

1) When I provide VBUS by PC host, it works fine when USB cable is plugged in. But, if USB not plugged in, the firmware is hang up. 

2) If I plugged in  USB cable, start running, then I can plug or unplug without any problem.

3) If I power USB by 5VDC, not from VBUS, it works fine...

Can anyone help me to debug where the problem is and how to fix it?

Thanks,

Christie

 

0 件の賞賛
返信
10 返答(返信)

6,047件の閲覧回数
a8Chcx
Contributor V

Hi,

I found the following cause the problem:

The MCU is stalling after command execution

static void USB_DeviceEhciSetDefaultState(usb_device_ehci_state_struct_t *ehciState){

...

hciState->registerBase->DEVICEADDR = 0U;

}

Can anyone help me how to fix the problem?

Thanks,

Christie

0 件の賞賛
返信

6,041件の閲覧回数
bobpaddock
Senior Contributor IV

Setting the USB Address to Zero at the start of enumeration is normal. That in itself isn't going to cause any issues.

What is the line before that doing?  Sometimes the debuggers can be off by a line when there is a fault.

What is powering the device when this happens?

Is there a bus fault trap set up that would show the address of any bus faults? Could something be invalid with ehciState in this power configuration?

 

0 件の賞賛
返信

6,038件の閲覧回数
a8Chcx
Contributor V

Another thing, it works fine if I remove set address command...

0 件の賞賛
返信

6,033件の閲覧回数
bobpaddock
Senior Contributor IV
That could cause odd issues with enumeration if the device is moved to another USB port or hub while it remains powered.
0 件の賞賛
返信

6,039件の閲覧回数
a8Chcx
Contributor V

Hi bobpaddock, 

Thanks.

If VREG_IN0, VREG_IN1, and USB1_VBUS of MCU are powered by 5V or Vbus(USB cable plugged in), it works fine.

If there is no power on VREG_IN0, VREG_IN1, and USB1_VBUS of MCU, it hangs on set address command. But, if I plug in USN cable, then it works again...

If there is any privilege to write this register(offset=0x0154)? Or need to enable something before writing to this register?

Thanks,

Christie

0 件の賞賛
返信

6,035件の閲覧回数
bobpaddock
Senior Contributor IV
So there is no power to the USB module then (Being independent of the chips power)? No way to tell what an unpowered module will do.

I don't know that chip specification to answer your other question. The general answer of Kienits line is 'no'.

0 件の賞賛
返信

5,997件の閲覧回数
a8Chcx
Contributor V

Hi bobpadock,

 

Yes. You are right. If there is power on VEG_IN0&1, it works fine.

I am using BUS_powered mode. If there is no power and should not initialize USB?

I have to know the USB1_VBUS pin status. Could you tell how to do that?

I am using usb_1.6.3 for K66F MCU for now?

Thanks,

Christie

0 件の賞賛
返信

5,993件の閲覧回数
a8Chcx
Contributor V

Hi,

My problem is:

In bus-power mode USB device, if no USB cable connected to Host, there is no power and I am hanging on set to the default address line. But, if no power, USB drive is not normal, I can't read the USB1_VBUS register, right?

Can anybody tell me how to get USB1_VBUS status? Can I read this register even without USB power?

I am using K66F MCU...

Thanks,

Christie

0 件の賞賛
返信

5,984件の閲覧回数
bobpaddock
Senior Contributor IV
The solution that has been recommended by NXP here in the past is a voltage divider to an I/O pin for VUSB detection.

0 件の賞賛
返信

5,982件の閲覧回数
a8Chcx
Contributor V

Hi bobpaddock,

Thanks.

Do you have any detail for this recommendation?

 

0 件の賞賛
返信