USB OTG connection diagram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB OTG connection diagram

ソリューションへジャンプ
2,356件の閲覧回数
javierhernande1
Contributor IV

Hello,

Is there an example of how to connect K2x MCU family to USB Type-C connector with OTG support? I have not found anything.

Best regards

usb.png

ラベル(2)
1 解決策
2,095件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javier,

If you need full USB type C function support, you have use some chip like CC logic for USB Type-C applications|NXP besides Kinetis K2x, but if you just need a USB type C connection, you may connect the signals that K2x USB FS OTG has and leave other unused signals unconnected.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,096件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javier,

If you need full USB type C function support, you have use some chip like CC logic for USB Type-C applications|NXP besides Kinetis K2x, but if you just need a USB type C connection, you may connect the signals that K2x USB FS OTG has and leave other unused signals unconnected.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,095件の閲覧回数
javierhernande1
Contributor IV

just at a USB type C connection.

Thanks very much.

0 件の賞賛
返信