USB-MSD Boot Loader OS compatibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB-MSD Boot Loader OS compatibility

1,284 次查看
mjbcswitzerland
Specialist V

Hi All

USB-MSD bootloaders have become very popular in the last few years but OS manufacturers are not always making life easy with their enhancements to the behavior when external hardware driver are connected - Windows 8.1 update added a well known tripping stone which doesn't allow older mbed loaders to operate correctly, or be updated to newer versions with workarounds, for instance.

However Windows 8.1 is almost harmless in comparison to MAC OS X.

The uTasker serial loader (including KBOOT compatibility and USB-MSD in parallel) and available for all K and KL devices with USB was of course also not saved a certain amount of agony to ensure compatibility. For the low-down on just what the MAC OS X does with SD cards and USB-MSD loaders and workarounds implemented see the following development story:

http://www.utasker.com/kinetis/USB-MSD-MAC.html

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

标记 (3)
0 项奖励
回复
0 回复数