USB-MSD Boot Loader OS compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB-MSD Boot Loader OS compatibility

1,273 Views
mjbcswitzerland
Specialist V

Hi All

USB-MSD bootloaders have become very popular in the last few years but OS manufacturers are not always making life easy with their enhancements to the behavior when external hardware driver are connected - Windows 8.1 update added a well known tripping stone which doesn't allow older mbed loaders to operate correctly, or be updated to newer versions with workarounds, for instance.

However Windows 8.1 is almost harmless in comparison to MAC OS X.

The uTasker serial loader (including KBOOT compatibility and USB-MSD in parallel) and available for all K and KL devices with USB was of course also not saved a certain amount of agony to ensure compatibility. For the low-down on just what the MAC OS X does with SD cards and USB-MSD loaders and workarounds implemented see the following development story:

http://www.utasker.com/kinetis/USB-MSD-MAC.html

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

Tags (3)
0 Kudos
Reply
0 Replies