USB K20 Regd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB K20 Regd

1,522件の閲覧回数
kathirkamuannak
Contributor II

Dear Sir/Madam,

I am using MK20DX128Vlf5 microcontroller for my USB project.I  am using usb_host:Host_STACK bean for my project. the interrupt priority defined in the generated file is below.

pastedImage_3.png

The problem is when I add extra periodic interrupts of 1ms and 15us and 15us(all are minimal priority). The usb code is not working properly when i put any snippet inside the ISRs of the interrupts. When I remove the snippet. The usb code is working properly(that the pendrive gets attached to the k20 controller). What goes wrong here?Please help me.

Thanks and Regards,

A.Kathirkamu

タグ(2)
0 件の賞賛
返信
1 返信

1,442件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi kathirkamu annakamu

Could you clarify:

What Stack version are you using?

You mentioned that you add interrupts, this mean that you specify another interruption or that you are modifying USB interrupt?

Could you share your project? or add more information of how your configure your project?

Regards

Jorge Alcala

0 件の賞賛
返信