USB Human Interface Device Boot Loader for Kinetis (AN4764)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Human Interface Device Boot Loader for Kinetis (AN4764)

Jump to solution
3,645 Views
DolomitiLynx
Contributor III

The application note AN4764 describes the use of a small footprint (4Kb) USB HID bootloader for Kinetis K and L uC. The document make explicit reference to a IAR project, named "kinetis_L_USB_HID_Bootloader\build\iar\kl25z_HID_Booltoader\kl25z_Lite_Bootloader.eww" and a program named "HIDBootloader.exe", where is available such material?

Thanks

1 Solution
2,773 Views
apanecatl
Senior Contributor II

I'm afraid the app note is quite recent and the code example has not been released, we expect it to be released in a short time however there is not a defined date for this to happen, in the mean time as Dosieto mentions, you could create one using Processor Expert

View solution in original post

0 Kudos
Reply
4 Replies
2,774 Views
apanecatl
Senior Contributor II

I'm afraid the app note is quite recent and the code example has not been released, we expect it to be released in a short time however there is not a defined date for this to happen, in the mean time as Dosieto mentions, you could create one using Processor Expert

0 Kudos
Reply
2,773 Views
dositeoescobars
Contributor II

Hi Gulio,

You are right, couldn't find the archives, but here is the link to another document that tells how to easily create one using Processor Expert: Serial Bootloader for the Freedom Board with Processor Expert | MCU on Eclipse

hope you find it useful.

Dositeo Escobar

2,773 Views
dositeoescobars
Contributor II

Hi Giulio,

Can you provide the link to the Application note?

Thanks

2,773 Views
DolomitiLynx
Contributor III

Here the link to the application note. It has been published in the Kinetis Documentation Section of the Freescale Site.

http://cache.freescale.com/files/32bit/doc/app_note/AN4764.pdf

Hope it can be useful for you.

Giulio

0 Kudos
Reply