USB Human Interface Device Boot Loader for Kinetis (AN4764)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Human Interface Device Boot Loader for Kinetis (AN4764)

ソリューションへジャンプ
3,774件の閲覧回数
DolomitiLynx
Contributor III

The application note AN4764 describes the use of a small footprint (4Kb) USB HID bootloader for Kinetis K and L uC. The document make explicit reference to a IAR project, named "kinetis_L_USB_HID_Bootloader\build\iar\kl25z_HID_Booltoader\kl25z_Lite_Bootloader.eww" and a program named "HIDBootloader.exe", where is available such material?

Thanks

1 解決策
2,902件の閲覧回数
apanecatl
Senior Contributor II

I'm afraid the app note is quite recent and the code example has not been released, we expect it to be released in a short time however there is not a defined date for this to happen, in the mean time as Dosieto mentions, you could create one using Processor Expert

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,903件の閲覧回数
apanecatl
Senior Contributor II

I'm afraid the app note is quite recent and the code example has not been released, we expect it to be released in a short time however there is not a defined date for this to happen, in the mean time as Dosieto mentions, you could create one using Processor Expert

0 件の賞賛
返信
2,902件の閲覧回数
dositeoescobars
Contributor II

Hi Gulio,

You are right, couldn't find the archives, but here is the link to another document that tells how to easily create one using Processor Expert: Serial Bootloader for the Freedom Board with Processor Expert | MCU on Eclipse

hope you find it useful.

Dositeo Escobar

2,902件の閲覧回数
dositeoescobars
Contributor II

Hi Giulio,

Can you provide the link to the Application note?

Thanks

2,902件の閲覧回数
DolomitiLynx
Contributor III

Here the link to the application note. It has been published in the Kinetis Documentation Section of the Freescale Site.

http://cache.freescale.com/files/32bit/doc/app_note/AN4764.pdf

Hope it can be useful for you.

Giulio

0 件の賞賛
返信