USB Host MSD Fatfs FreeRTOS Example Problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Host MSD Fatfs FreeRTOS Example Problems

4,021件の閲覧回数
Microfelix
Contributor IV

hi, i am using K66 and freertos sdk 2.10.0.
I am working on USB with fatfs and freertos. During the development of my project I realized that every now and then the reading of a USB file fails.
So I created a routine that continuously reads a file and after several reads it goes into error giving "DISK_ERROR"

Help me

Maurizio

 

0 件の賞賛
返信
4 返答(返信)

4,014件の閲覧回数
Microfelix
Contributor IV

what I noticed from the tests is that this kind of error occurs if I insert other "ENET lwip" work tasks in the project.
As soon as this task is activated, errors become very frequent.
While if, I disable it, there are + no errors and it completes many readings

 

Maurizio

0 件の賞賛
返信

3,993件の閲覧回数
bobpaddock
Senior Contributor III

USB can be Interrupt intense.
Could lwip be disabling IRQs too long?

 

0 件の賞賛
返信

3,965件の閲覧回数
Microfelix
Contributor IV

hi,
it seems that the problem occurs more frequently when I have large files.
With small files the problem is not there.

Any solution?

 

Maurizio

0 件の賞賛
返信

3,987件の閲覧回数
Microfelix
Contributor IV

I thought about this. In fact I tried to change the IRQ values. I changed the priorities of the usb which was originally 6. I took it to a lower level and nothing has changed. I tried to raise it a lot, and it seems to be doing better but it still goes wrong.

Is there any other way to fix?
Is it possible that while you are working the usb, the other interrupts go to the queue?

 

Maurizio

0 件の賞賛
返信