USB FS demo code without any RTOS for Kinetis K60/K61/K70 .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB FS demo code without any RTOS for Kinetis K60/K61/K70 .

1,213件の閲覧回数
virendrapatel
Contributor III

Hi Freescale/NXP,

Can anyone please provide me a demo code without any RTOS for USB Full Speed for Kinetis K60/K61/K70?

BR,

Virendra

ラベル(2)
0 件の賞賛
返信
1 返信

1,073件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Virendra

Here you can find example codes for Kinetis 120 MHz. In these examples, you will find some example for K70 board using CW or IAR. K70_120 |Kinetis K70 120/150 MHz MCUs|NXP

Go to software & tools tab, then look for snippets, Boot Code, Headers, Monitors, etc section and then download the Kinetis 120MHz bare metal sample code (REV 1.4)

I hope this can help you.

Best Regards,

Isaac

----------------------------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信