USB FS demo code without any RTOS for Kinetis K60/K61/K70 .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB FS demo code without any RTOS for Kinetis K60/K61/K70 .

1,222 Views
virendrapatel
Contributor III

Hi Freescale/NXP,

Can anyone please provide me a demo code without any RTOS for USB Full Speed for Kinetis K60/K61/K70?

BR,

Virendra

Labels (2)
0 Kudos
Reply
1 Reply

1,082 Views
isaacavila
NXP Employee
NXP Employee

Hello Virendra

Here you can find example codes for Kinetis 120 MHz. In these examples, you will find some example for K70 board using CW or IAR. K70_120 |Kinetis K70 120/150 MHz MCUs|NXP

Go to software & tools tab, then look for snippets, Boot Code, Headers, Monitors, etc section and then download the Kinetis 120MHz bare metal sample code (REV 1.4)

I hope this can help you.

Best Regards,

Isaac

----------------------------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply