USB Driver for MK60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Driver for MK60N512

1,186件の閲覧回数
karthikpoojary
Contributor III

I am using USB v3.2.0  stack.

Steps I followed

1. Navigate to the project folder (s08usbjm60) and locate the CodeWwarrior10 project file (.project).

2. Open the project by dragging the .project file and dropping it into the CodeWarrior 10 project

space.

3. After you have opened the project, the following window appears. To build the project choose

"Build Project" from the Project menu.

And here I am getting following error.

DescriptionResourcePathLocationType
make: *** [Source/driver/usb_dci_c.obj] Error 1s08usbjm60line 0C/C++ Problem
タグ(2)
1 返信

1,107件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Karthik,

I'd like to suggest that you should check whether the CW10.1 had already installed the package that be applicable to S08 or not.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------