USB Driver for MK60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Driver for MK60N512

1,217 Views
karthikpoojary
Contributor III

I am using USB v3.2.0  stack.

Steps I followed

1. Navigate to the project folder (s08usbjm60) and locate the CodeWwarrior10 project file (.project).

2. Open the project by dragging the .project file and dropping it into the CodeWarrior 10 project

space.

3. After you have opened the project, the following window appears. To build the project choose

"Build Project" from the Project menu.

And here I am getting following error.

DescriptionResourcePathLocationType
make: *** [Source/driver/usb_dci_c.obj] Error 1s08usbjm60line 0C/C++ Problem
1 Reply

1,138 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Karthik,

I'd like to suggest that you should check whether the CW10.1 had already installed the package that be applicable to S08 or not.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------