UARTx_C2 send break?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UARTx_C2 send break?

1,798 次查看
danielchai
Senior Contributor I

Hi All,

For K60, the UARTx_C2 SBK bit is used to send break.

Does it mean when I set the SBK bit, it will send break continuously until I clear the SBK bit?

Or it means after SBK is set, it only send 10, 11, 12, 13 or 14 logic 0s no matter if SBK is cleared or not?

Thank you.

-Daniel

0 项奖励
回复
2 回复数

1,590 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Daniel chai,

  Thank you for your question in our communty.

    As our reference manual said,

59.jpg

60.jpg

so, it will continuoulsly send break until you clear the SBK bit.

Wish my answer helps you!

If you still have question, please contact with me!

Best regards!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,590 次查看
mjbcswitzerland
Specialist V

Daniel

If you set the SBK bit the UART will continuously send break characeters until you remove the bit. Then it will complete sending the break character that it was in the process of sending before returning to the idle line state.

Regards

Mark

0 项奖励
回复