UART communication with Putty

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART communication with Putty

ソリューションへジャンプ
5,138件の閲覧回数
songja
Contributor III

Hi,

I am printing 8 ADC values out to Putty and save the log file as "*.csv".

But when I checked the printed values, there are no taps between them even though I added '\t'.

for example, if the values were "1, 2 3, 4, 5, 6, 7, 8", the saved value in CSV file is "12345678".

I am using FreeRTOS  and the code is attached below.

I also tried to print all the values together with one variable. 

void uart_task(void)
{
      char TEMP[32];

      TickType_t xLastWakeTime;

      uart_config.srcclk = DEMO_UART_CLK_FREQ;
      uart_config.base = DEMO_UART;

      UART_RTOS_Init(&handle, &t_handle, &uart_config);

      

      for(;;)

      {
            xLastWakeTime = xTaskGetTickCount();

            for (int i = 0; i < NOS; i++ )

            {
                  sprintf(TEMP, "%d",OFFSET[i]-ADC_VALs[i]);
                  UART_RTOS_Send(&handle, (uint8_t *)TEMP, strlen(TEMP))

            }

      UART_RTOS_Send(&handle, "\r\n", strlen("\r\n"));
      vTaskDelayUntil(&xLastWakeTime, 20);
      }
UART_RTOS_Deinit(&handle);
vTaskSuspend(NULL);
}

Thanks,

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
4,703件の閲覧回数
songja
Contributor III

Hi Kerry,

I was saving the data as "printable output" via Putty and I changed it to "All session output".

Moreover, saving the data as '*.csv' causes the problem as well (The format somewhat collapsed).

Once I use "All session output" and save the data as '*.txt', it works fine.

Thank you very much for your help!

Jay

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,703件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi JAEYONE SONG,

    You can change a PC serial terminal software to receive the data, whether it have the tab or not.

    I think this problem should caused by the PC putty.

    After you receive the data in the terminal, you can copy the data, then save it to the file .csv.

    Please try it again.

    If you still have problem about it, please tell me what the kinetis chip you are using now, tell me the partnumber.

    Besides, you also need to give me the PC side received data, then give me the screen shoot about your problem .csv.

   


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,704件の閲覧回数
songja
Contributor III

Hi Kerry,

I was saving the data as "printable output" via Putty and I changed it to "All session output".

Moreover, saving the data as '*.csv' causes the problem as well (The format somewhat collapsed).

Once I use "All session output" and save the data as '*.txt', it works fine.

Thank you very much for your help!

Jay

0 件の賞賛
返信
4,703件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jay,

    Good!

So, if the problem is solved, please help me to mark the correct answer, just to close this case, thank you!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信