UART Flash programming KE02Z MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART Flash programming KE02Z MCU

2,001 次查看
rikipatel
Contributor I

Hello All,

I wanted to select the MKE02Z64VLD2 MCU for my application wherein mainly the peripherals would be connected to UART.

I was going through flash programming section, preferably, I would like to program the flash using UART port and a  USB to TTL converter connected to PC and some UI of Freescale.

I referred document 1) "AN2295.pdf" and 2) Getting started with ROM bootloader.PDF", the second says programing the flash with UART but does not mention the UART number, I assume UART0 for the same. Kindly confirm.

If anyone could confirm the above and share some reference schematic.

Regards

Riki Patel

0 项奖励
回复
1 回复

1,715 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Riki Patel,

FRDM-KE02Z has provided the sample code package, and in the sample package, Bootloader_sci demo can work with the AN2295 PC bootloader application.

So I'd highly recommend you to have a try.

FRDM-KE02Z sample code package:

https://www.nxp.com/webapp/sps/download/preDownload.jsp

I've also attached the AN2295 PC bootloader application.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复