UART FIFO Tx mode MK53DN512VLQ10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART FIFO Tx mode MK53DN512VLQ10

1,514 Views
nenadmitic
Contributor I

Hi,

we want to enable UART1 transmitter on MK53DN512VLQ10 to transmit data with FIFO functionality using interrupt-driven software approach and we have problem.

We have done next in initialization phase:

-    enable transmit FIFO with setting UART1_PFIFO[TXFE]

-    flushed transmit FIFO buffer with setting UART1_CFIFO[TXFLUSH]

-    set TXWATER to 0

-    enable transmitter with setting UART1_C2[TE]

When we want to start transmission we set UART1_C2[TIE].

In every UART1 interrupt service routine we write TXFIFOSIZE(8) datawords in UART1_D register. In last UART1 interrupt service routine we write less than or equal TXFIFOSIZE datawords in UART1_D register and then we reset UART1_C2[TIE]. We read UART1_S1 register before every write dataword to UART1_D in interrupt service routine in order to clear UART1_S1[TDRE] flag.

In some cases UART1 generates interrupt service routine even when transmit FIFO buffer is not empty, even we set UART1_TWFIFO[TXWATER] = 0 in initialization phase. In these cases UART1 generates interrupt service routine even when UART1_S1[TDRE] is not set and when UART1_SFIFO[TXEMPT] is not set.

Please for help.

Please sent us properly example for using FIFO functionality of UART peripheral.

Best Regards,

Nenad

Labels (1)
0 Kudos
Reply
1 Reply

1,218 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Nenad,

Please check attached Kinetis UART FIFO function test code.

Wish it helps.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply