UART Error on KL26Z128 using CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART Error on KL26Z128 using CodeWarrior

Jump to solution
6,856 Views
omarvallecasas
Contributor III

Hi,

I'm having a issue when I try to read I2C with FXOS8700, and put it into board UART1, to visualize by Computer Serial Terminal. Is there any communication protocol to communicate between UART and OpenSDA? I attached code with the issue.

 

Thanks in advance,

 

Omar Valle Casas

Original Attachment has been moved to: inercial20.rar

1 Solution
6,180 Views
EarlOrlando
Senior Contributor II

Update:

The UART Module Clock is the bus clock which does not seem to be configured. By default the Bus Clock is 20.97152 MHz, so:

SBR = 20.97152 MHz / (16 * 115200) = 11.3777

I suggest to change the bus clock to 48 MHz, it will produce a more accurate baud rate:

SBR = 48 MHz / (16 * 115200) = 26.0416

View solution in original post

10 Replies
6,180 Views
EarlOrlando
Senior Contributor II

Hello Omar,

In the FRDM-KL26Z schematic​ (I suppose you are using a freedom board) you can see that the OpenSDA UART is routed to the PTC3 and PTC4 pins (UART1).

pastedImage_4.png

In the KL26P121M48SF4RM Reference Manual​ pinout you can see that the PTC3 and PTC4 pins are disabled by default. You need to  select the alternative 3 in both cases in the PORTC_PCRx[MUX] register.

pastedImage_8.png

pastedImage_7.pngpastedImage_6.png

Best regards,

Earl Orlando.

/* If this post answers your question please click over the ​Correct Answer​ button. */

6,180 Views
omarvallecasas
Contributor III

Hi, I configured the SIM for Port enabling and didn't worked. I'm putting code inside message body to facilitate visualization.

void uart1_init (void){

  /*habilitando o clock para a UART0 (pg.221)*/

  SIM_SCGC4 = SIM_SCGC4_UART1_MASK;

  SIM_SOPT5 |= SIM_SOPT5_UART1TXSRC(0);

  

  PORTC_PCR3 = PORT_PCR_MUX(0x3); // Omar's 08_07_15

  PORTC_PCR4 = PORT_PCR_MUX(0x3); // Omar's 08_07_15

  

    UART1_BDH = 0x02;

    UART1_BDL = 0x71; /* SBR = 26 */

  //   UART1_C4 = 0x03; /* OSR = 4 */   //Não existe

   

    UART1_C2 |= UART0_C2_TE_MASK;

   

    UART1_D  = 2;

  

}

   

    /*---------------------------------------------------------------------*/

  /*                       ENVIA DADO PELA SERIAL                        */

  /*---------------------------------------------------------------------*/

void uart1_send (int i2c1_data){

  /*Se a flag de transmissao TDRE (pg.761) estiver igual a zero (buffer cheio), não deve fazer nada*/

     while(!(UART1_S1&UART_S1_TDRE_MASK) && !(UART1_S1&UART_S1_TC_MASK));

     UART1_D  = i2c1_data;

    

}

  /*---------------------------------------------------------------------*/

  /*                         INICIALIZACAO DA I2C                        */

  /*---------------------------------------------------------------------*/

void i2c_init(void){

  /* O registrador System Clock Gating Control Register 4 (SIM_SCGC4) eh responsavel por habilitar o clock da I2C0 (pg.220) */

  SIM_SCGC4 |= SIM_SCGC4_I2C0_MASK;

  /* O registrador System Clock Gating Control Register 5 (SIM_SCGC5) eh responsavel por habilitar o clock da PORTE (pg.222)*/

  SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK|SIM_SCGC5_PORTC_MASK|SIM_SCGC5_PORTA_MASK;

  /* O pino SCL do FSXO8700CQ está conectado ao PTE24 do KL26Z128 ---> CONFIGURACAO DE PTE24 = SCL : */

  /* Pela tabela de Pinout (pq.176) , PTE24 = I2C0_SCL no modo ALT5 (0x5) */

  PORTC_PCR24 |= PORT_PCR_MUX(0x5);

  /* O pino SDA do FSXO8700CQ está conectado ao PTE25 do KL26Z128 ---> CONFIGURACAO DE PTE25 = SDA : */

  /* Pela tabela de Pinout (pq.176) , PTE25 = I2C0_SDA no modo ALT5 (0x5) */

  PORTC_PCR24 |= PORT_PCR_MUX(0x5);

  /*O registrador Frequency Divider Register (I2C0_F) [I2C memory map, pg.722] recebe a frequência de operacao da I2C */

  /*O I2C0_F deve receber o Clock Rate (ICR) [pg.723] . Neste caso : 0x14 ---> SDA hold time = 2.125us, SCL start hold time = 4.25us, SCL stop hold time = 5.125us */

  I2C0_F |= I2C_F_ICR(0X14);

  /* O registrador I2C Control Register 1 (I2C0_C1) [I2C memory map, pg.722] eh responsavel por habilitar a I2C0 */

  /* Para habilitar , o bit IICEN (bit 7) [pg.724] deve ser setado (0x80) */

  I2C0_C1 |= I2C_C1_IICEN_MASK;

  /*------------------------------------------------------------------------------------------*/

  /*     CONFIGURACAO DE PTD0 PARA A INTERRUPCAO DE BORDA DE DESCIDA (INT1) DO FXOS8700CQ     */

  /*------------------------------------------------------------------------------------------*/

  /* O registrador System Clock Gating Control Register 5 (SIM_SCGC5) eh responsavel por habilitar o clock da PORTD (pg.222)*/

  SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK;

  /*  O registrador Interrupt Status Flag Register (PORTx_ISFR) [pg.202] eh zerado, PTD0 é configurado como GPIO e como INT1*/

  PORTD_PCR0 |= (0|PORT_PCR_ISF_MASK| // Limpa a flag

  PORT_PCR_MUX(0x1)| // PTD4 eh configurado como GPIO [MUX, tabela pg.200]

  PORT_PCR_IRQC(0xA)); // PTD4 eh configurado como interrupcao de borda de descida (0xA) [IRQC, tabela pg.200]

  /*Habilitando a configuracao Nested Vectored Controller (NVIC) [pg.57] na porta D */

  NVIC_ICPR |= 1 << ((INT_PORTC_PORTD - 16)%32);

  NVIC_ISER |= 1 << ((INT_PORTC_PORTD - 16)%32);

 

}

/*---------------------------------------------------------------------*/

/*                      ESPERA                  I2C                    */

/*---------------------------------------------------------------------*/

void i2c_wait(void){

  while(!(I2C0_S & I2C_S_TCF_MASK) );

}

/*---------------------------------------------------------------------*/

/*                      start                  I2C                    */

/*---------------------------------------------------------------------*/

void i2c_start(void){

  i2c_wait();

  I2C0_C1 = I2C_C1_TX_MASK;

}

/*---------------------------------------------------------------------*/

/*                      RESTART                  I2C                    */

/*---------------------------------------------------------------------*/

void i2c_restart(void){

  i2c_wait();

  I2C0_C1 = I2C_C1_RSTA_MASK;

}

/*---------------------------------------------------------------------*/

/*                      FECHA A TRANSMISSAO VIA I2C                    */

/*---------------------------------------------------------------------*/

void i2c_stop(void){

  i2c_wait();

  I2C0_FLT = I2C_FLT_SHEN_MASK;

}

/*---------------------------------------------------------------------*/

/*                      ESCREVE VIA I2C                    */

/*---------------------------------------------------------------------*/

void i2c_write(int data){

  i2c_wait();

  I2C0_D = data;

}

/*---------------------------------------------------------------------*/

/*                      LEITURA VIA I2C                    */

/*---------------------------------------------------------------------*/

int i2c_read(void){ 

  int i2c_read_data;

  i2c_wait();

  I2C0_S = I2C_S_SRW_MASK;

  i2c_wait();

  i2c_read_data = I2C0_D;

  return i2c_read_data;

}

/*---------------------------------------------------------------------*/

/*                      ENDEREÇAMENTO   VIA     I2C                    */

/*---------------------------------------------------------------------*/

void i2c_slaveREG_address(unsigned char addr){ 

  i2c_wait();

  I2C0_D = addr;

}

/*---------------------------------------------------------------------*/

/*                      INICIALIZACAO DO FXOS87OOCQ                    */

/*---------------------------------------------------------------------*/

void fxos8700cq_init (void) {

  /* Setando FXOS8700CQ como slave

  *

  * Dos headers:

  *

  * DEFINIÇÃO DO ENDEREÇO DO FXOS8700CQ COMO ESCRAVO

  * #define FXOS8700CQ_SLAVE_ADDR 0x1E --> SA0=0, SA1=0

  */

  I2C0_A1 = FXOS8700CQ_SLAVE_ADDR;

  /*CTRL_REG2 --> initiate a software reset;

  *

  * bits

  * [0,1]: mods = 0b00 (normal) -->  determines the Wake mode power and noise for acceleration measurements.

  * [2]  : slpe = 0 --> Auto-sleep is not enable.

  * [3,4]: smods = 0b00 (normal) -->  determines the Sleep mode power and noise for acceleration measurements.

  * [5]  : not used.

  * [6]  : rst = 1 --> Device reset enabled.

  * [7]  : st  = 0 --> accelerometer self-test disabled.

  */

  i2c_start();

  i2c_slaveREG_address(CTRL_REG2); // COLOCA O ENDEREÇO DO REGISTRADOR DO FXOS NO BARRAMENTO DE DADOS

  i2c_write(0X40); //ESCREVE NO REGISTRADOR

  

  /*M_CTRL_REG1 --> Magnetic control register; set hybrid mode;

  *

  * bits

  * [0,1]  : m_hms = 0b11 -->  Hybrid mode, both accelerometer and magnetometer sensors are active.

  * [2,3,4]: m_os = 0b111 --> 4xOSR (for 400Hz).

  * [5]    : m_ost = 0 --> one-shot magnetic complete.

  * [6]    : m_rst = 1 --> one-shot magnetic reset is enabled, hardware cleared when complete.

  * [7]    : m_acal = 0 -->  auto-calibration feature disabled.

  */

  i2c_restart();

  i2c_slaveREG_address(CTRL_REG1); // COLOCA O ENDEREÇO DO REGISTRADOR DO FXOS NO BARRAMENTO DE DADOS

  i2c_write(0X5F); //ESCREVE NO REGISTRADOR

  

  /*M_CTRL_REG2 --> Magnetic measurement features

  *

  * bit

  * [0,1] : m_rst_cnt = 0b00 -->  Automatic magnetic reset at the beginning of each ODR cycle (default).

  * [2]   : m_maxmin_rst = 0 --> Magnetic measurement min/max detection function reset:: No reset sequence is active.

  * [3]   : m_maxmin_dis_ths = 0 --> Magnetic measurement min/max detection function disable using the magnetic threshold event trigger: No impact to magnetic min/max detection function on a magnetic threshold event.

  * [4]   : m_maxmin_dis = 0 -->  Magnetic min/max detection function is enabled (default).

  * [5]   : hyb_autoinc_mode = 1 --> hybrid mode enable.

  * [6,7] : not used.

  */

  i2c_restart();

  i2c_slaveREG_address(M_CTRL_REG2); // COLOCA O ENDEREÇO DO REGISTRADOR DO FXOS NO BARRAMENTO DE DADOS

  i2c_write(0X20); //ESCREVE NO REGISTRADOR

  

  /*CTRL_REG1 --> initial data features

  *

  * bits

  * [0]     : active = 1 --> active mode.

  * [1]     : f_read = 0 --> fast-read mode disable, will work in normal mode.

  * [2]     : lnoise = 1 --> reduced noise mode.

  * [3,4,5] : dr = 0b000 --> Output Data Rate (ODR) for hybrid mode (400 Hz).

  * [6,7]   : aslp_rate = 0b00 --> Configures the auto-wake sample frequency when the device is in Sleep mode (50 Hz).

  */

  i2c_restart();

  i2c_slaveREG_address(CTRL_REG1); // COLOCA O ENDEREÇO DO REGISTRADOR DO FXOS NO BARRAMENTO DE DADOS

  i2c_write(0X05); //ESCREVE NO REGISTRADOR

  

  /*XYZ_DATA_CFG -->The XYZ_DATA_CFG register is used to configure the desired acceleration full-scale range, and also to select whether the output data is passed through the high-pass filter.

  *

  * bits

  * [0,1]   : fs = 0b01 -->  Accelerometer full-scale range selection (+- 0.488 mg/LSB)

  * [2,3]   : not used.

  * [4]     : hpf_out = 0 --> high pass filter disabled.

  * [5,6,7] : not used

  */

  

  i2c_restart();

  i2c_slaveREG_address(XYZ_DATA_CFG_REG); // COLOCA O ENDEREÇO DO REGISTRADOR DO FXOS NO BARRAMENTO DE DADOS

  i2c_write(0X02); //ESCREVE NO REGISTRADOR

  

  i2c_stop();

  

}

/*---------------------------------------------------------------------*/

/*                              FUNCAO MAIN                            */

/*---------------------------------------------------------------------*/

int main(void)

{

  uart1_init();

  i2c_init();

  fxos8700cq_init();

  i2c_start();

      

  while(1)

  {

  i2c_restart();

 

  uart1_send(  i2c_read());

 

  }

  return 0;

}

Maybe someone can give me a clue.

0 Kudos
Reply
6,180 Views
EarlOrlando
Senior Contributor II

Do you have an oscilloscope to see the signals in the PTC3 and PTC4 pins? This just to be sure that the baudrate is ok.

Does the program work ok except for the UART transmissions or does it go to the default handler function?

Also, please enable the clock gate for the PORTC before its initialization.

SIM_SCGC5  |= SIM_SCGC5_PORTC_MASK;

Best regards,

Earl.

6,180 Views
omarvallecasas
Contributor III

Hi Orlando, I enabled PORTC for first and measured UART on the board, PTC = '1' (3.3 V DC) and PTC4 = 10.2 kHz (Square '1'=3.3 V, '0'= 0 V). I try to see Registers values in Debug's window, and UART1_D remain in 0x00. At the begining it went to the default handler function error, now it doesn't write nothing on UART1.

Regards,

Omar

0 Kudos
Reply
6,180 Views
EarlOrlando
Senior Contributor II

Hi Omar,

Does the UART_TX (PTC4) signal completely square or does it seem to be an UART signal? If it seems to be an UART signal maybe the problem is the baudrate. Also, I think that you will see some data in the UART_D register only when you receive data.

Regards,

Earl.

6,180 Views
omarvallecasas
Contributor III

It really seems like a UART signal, do you know the right boudrate configuration I'm using or think I'm using 115200 for UART1_BDH = 0x00 and UART1_BDL = 0x1A. Is it right?

Thanks and regards,

Omar

0 Kudos
Reply
6,180 Views
EarlOrlando
Senior Contributor II

Hello Omar,

In the reference manual you can see that the baudrate is generated as follows:

pastedImage_0.png

So the SBR value can be calculated:

SBR[12:0] = UART Module Clock / (16 * Baudrate)

The UART Module Clock is the bus clock which does not seem to be configured.

Best regards,

Earl.

6,181 Views
EarlOrlando
Senior Contributor II

Update:

The UART Module Clock is the bus clock which does not seem to be configured. By default the Bus Clock is 20.97152 MHz, so:

SBR = 20.97152 MHz / (16 * 115200) = 11.3777

I suggest to change the bus clock to 48 MHz, it will produce a more accurate baud rate:

SBR = 48 MHz / (16 * 115200) = 26.0416

6,180 Views
omarvallecasas
Contributor III

Hi Earl,

I achieved putting the right Baud Rate and the UART has started to function. Now I'm trying to configure right the I2C0 for FX0S7800 reading. UART will serve to have a feedback.

Thanks so much,

Omar

0 Kudos
Reply
6,180 Views
vipinkumar27
Contributor II

Hi ,

I have just started coding for kl26z board.

I have to use two uarts -lpsci(UART0) and UART1.

Lpsci driver is working fine .I tried writing uart driver for uart1 using the structure of lpsci.

I don't know why uart1 is not working . At first, I tried with pin nos PTE-22 and 23 as given in Pinout schematic .

After going through this conversation ,I changed the pins to PTC3  and PTC4 for Uart1 tx and Rx.

I tried changing the Uart clock but I dont know its not changing and everytime,its showing 12MHZ.

What could be the problem ?

Please suggest me something.

0 Kudos
Reply