UART DMA and CTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART DMA and CTS

Jump to solution
2,649 Views
lsrbigfoot
Contributor IV

Does the UART-CTS input signal (when activated) have the ability to block/unblock UART-Tx DMA traffic automatically (without processor intervention)?

If not, then what extra controls are required to make this happen?

Labels (1)
0 Kudos
Reply
1 Solution
2,475 Views
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

View solution in original post

0 Kudos
Reply
1 Reply
2,476 Views
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

0 Kudos
Reply