UART DMA and CTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,707件の閲覧回数
lsrbigfoot
Contributor IV

Does the UART-CTS input signal (when activated) have the ability to block/unblock UART-Tx DMA traffic automatically (without processor intervention)?

If not, then what extra controls are required to make this happen?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,533件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,534件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

0 件の賞賛
返信