UART Array Transfer Using DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART Array Transfer Using DMA

ソリューションへジャンプ
2,448件の閲覧回数
ohiogt
Contributor III

I'm trying to transfer an array on at fixed intervals over the UART using DMA.  Sample code is below.  The code below only appears to transmit the first byte of the array, with other bytes mixed in sporadically.  I'm not sure if I need the FIFO setup or if I'm missing something else.  Any help would be appreciated.

Shawn

#define UART_BUFFER_LENGTH 9

uint32_t g_UARTBuf[9] = {0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53};

void InitUART(void)

{

UART0->C2 &= ~(UART_C2_TCIE_MASK | UART_C2_RIE_MASK | UART_C2_ILIE_MASK |

UART_C2_RE_MASK | UART_C2_RWU_MASK | UART_C2_SBK_MASK |

UART_C2_TIE_MASK | UART_C2_TE_MASK);

UART0->BDH &= ~(UART_BDH_LBKDIE_MASK | UART_BDH_RXEDGIE_MASK |

UART_BDH_SBR_MASK);

UART0->BDL &= ~(UART_BDL_SBR_MASK);

UART0->BDL |= UART_BDL_SBR(65U);

UART0->C1 &= ~(UART_C1_LOOPS_MASK | UART_C1_UARTSWAI_MASK | UART_C1_M_MASK |

UART_C1_ILT_MASK | UART_C1_PE_MASK);

UART0->C3 &= ~(UART_C3_TXINV_MASK | UART_C3_ORIE_MASK | UART_C3_NEIE_MASK |

UART_C3_FEIE_MASK | UART_C3_PEIE_MASK);

UART0->C4 &= ~(UART_C4_MAEN1_MASK | UART_C4_MAEN2_MASK | UART_C4_M10_MASK |

UART_C4_BRFA_MASK);

UART0->C4 |= UART_C4_BRFA(3U);

UART0->C5 &= ~(UART_C5_RDMAS_MASK);

UART0->C5 |= UART_C5_TDMAS_MASK;

UART0->MODEM &= ~(UART_MODEM_RXRTSE_MASK | UART_MODEM_TXRTSPOL_MASK |

UART_MODEM_TXRTSE_MASK | UART_MODEM_TXCTSE_MASK);

UART0->IR &= ~(UART_IR_IREN_MASK);

UART0->PFIFO &= ~(UART_PFIFO_TXFE_MASK | UART_PFIFO_TXFIFOSIZE_MASK |

UART_PFIFO_RXFE_MASK | UART_PFIFO_RXFIFOSIZE_MASK);

UART0->CFIFO &= ~(UART_CFIFO_RXOFE_MASK | UART_CFIFO_TXOFE_MASK |

UART_CFIFO_RXUFE_MASK);

UART0->CFIFO |= (UART_CFIFO_TXFLUSH_MASK | UART_CFIFO_RXFLUSH_MASK);

UART0->C7816 &= ~(UART_C7816_ONACK_MASK | UART_C7816_ANACK_MASK |

UART_C7816_INIT_MASK | UART_C7816_TTYPE_MASK | UART_C7816_ISO_7816E_MASK);

UART0->C2 |= (UART_C2_TIE_MASK | UART_C2_TE_MASK);

}

...

DMA0->TCD[2].CSR &= ~(DMA_CSR_BWC_MASK | DMA_CSR_MAJORELINK_MASK |

DMA_CSR_ESG_MASK | DMA_CSR_DREQ_MASK | DMA_CSR_INTHALF_MASK |

DMA_CSR_DONE_MASK | DMA_CSR_INTMAJOR_MASK);

DMA0->TCD[2].CSR |= DMA_CSR_BWC(3U);

DMA0->TCD[2].SADDR = (uint32_t)(&g_UARTBuf[0]);

DMA0->TCD[2].SOFF = 4U;

DMA0->TCD[2].ATTR = 0x0200;

DMA0->TCD[2].NBYTES_MLNO = (4)*(UART_BUFFER_LENGTH);

DMA0->TCD[2].SLAST = (-4)*(UART_BUFFER_LENGTH);;

DMA0->TCD[2].DADDR = (uint32_t)&(UART0->D);

DMA0->TCD[2].DOFF = 0;

DMA0->TCD[2].CITER_ELINKNO = 1;

DMA0->TCD[2].DLAST_SGA = 0;

DMA0->TCD[2].BITER_ELINKNO = 1;

DMA0->TCD[2].CSR |= DMA_CSR_DREQ_MASK;

...

DMA0->SERQ = 2U;

... (Below inside while loop)

if (Count < Timer)

{

Count++;

}

else

{

Count = 0;

DMA0->SERQ = 2U;

}

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,139件の閲覧回数
ohiogt
Contributor III

Disregard, I should have set the major loop counter to the number of bytes I needed to transmit.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,140件の閲覧回数
ohiogt
Contributor III

Disregard, I should have set the major loop counter to the number of bytes I needed to transmit.

0 件の賞賛
返信