UART Array Transfer Using DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART Array Transfer Using DMA

Jump to solution
2,566 Views
ohiogt
Contributor III

I'm trying to transfer an array on at fixed intervals over the UART using DMA.  Sample code is below.  The code below only appears to transmit the first byte of the array, with other bytes mixed in sporadically.  I'm not sure if I need the FIFO setup or if I'm missing something else.  Any help would be appreciated.

Shawn

#define UART_BUFFER_LENGTH 9

uint32_t g_UARTBuf[9] = {0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53};

void InitUART(void)

{

UART0->C2 &= ~(UART_C2_TCIE_MASK | UART_C2_RIE_MASK | UART_C2_ILIE_MASK |

UART_C2_RE_MASK | UART_C2_RWU_MASK | UART_C2_SBK_MASK |

UART_C2_TIE_MASK | UART_C2_TE_MASK);

UART0->BDH &= ~(UART_BDH_LBKDIE_MASK | UART_BDH_RXEDGIE_MASK |

UART_BDH_SBR_MASK);

UART0->BDL &= ~(UART_BDL_SBR_MASK);

UART0->BDL |= UART_BDL_SBR(65U);

UART0->C1 &= ~(UART_C1_LOOPS_MASK | UART_C1_UARTSWAI_MASK | UART_C1_M_MASK |

UART_C1_ILT_MASK | UART_C1_PE_MASK);

UART0->C3 &= ~(UART_C3_TXINV_MASK | UART_C3_ORIE_MASK | UART_C3_NEIE_MASK |

UART_C3_FEIE_MASK | UART_C3_PEIE_MASK);

UART0->C4 &= ~(UART_C4_MAEN1_MASK | UART_C4_MAEN2_MASK | UART_C4_M10_MASK |

UART_C4_BRFA_MASK);

UART0->C4 |= UART_C4_BRFA(3U);

UART0->C5 &= ~(UART_C5_RDMAS_MASK);

UART0->C5 |= UART_C5_TDMAS_MASK;

UART0->MODEM &= ~(UART_MODEM_RXRTSE_MASK | UART_MODEM_TXRTSPOL_MASK |

UART_MODEM_TXRTSE_MASK | UART_MODEM_TXCTSE_MASK);

UART0->IR &= ~(UART_IR_IREN_MASK);

UART0->PFIFO &= ~(UART_PFIFO_TXFE_MASK | UART_PFIFO_TXFIFOSIZE_MASK |

UART_PFIFO_RXFE_MASK | UART_PFIFO_RXFIFOSIZE_MASK);

UART0->CFIFO &= ~(UART_CFIFO_RXOFE_MASK | UART_CFIFO_TXOFE_MASK |

UART_CFIFO_RXUFE_MASK);

UART0->CFIFO |= (UART_CFIFO_TXFLUSH_MASK | UART_CFIFO_RXFLUSH_MASK);

UART0->C7816 &= ~(UART_C7816_ONACK_MASK | UART_C7816_ANACK_MASK |

UART_C7816_INIT_MASK | UART_C7816_TTYPE_MASK | UART_C7816_ISO_7816E_MASK);

UART0->C2 |= (UART_C2_TIE_MASK | UART_C2_TE_MASK);

}

...

DMA0->TCD[2].CSR &= ~(DMA_CSR_BWC_MASK | DMA_CSR_MAJORELINK_MASK |

DMA_CSR_ESG_MASK | DMA_CSR_DREQ_MASK | DMA_CSR_INTHALF_MASK |

DMA_CSR_DONE_MASK | DMA_CSR_INTMAJOR_MASK);

DMA0->TCD[2].CSR |= DMA_CSR_BWC(3U);

DMA0->TCD[2].SADDR = (uint32_t)(&g_UARTBuf[0]);

DMA0->TCD[2].SOFF = 4U;

DMA0->TCD[2].ATTR = 0x0200;

DMA0->TCD[2].NBYTES_MLNO = (4)*(UART_BUFFER_LENGTH);

DMA0->TCD[2].SLAST = (-4)*(UART_BUFFER_LENGTH);;

DMA0->TCD[2].DADDR = (uint32_t)&(UART0->D);

DMA0->TCD[2].DOFF = 0;

DMA0->TCD[2].CITER_ELINKNO = 1;

DMA0->TCD[2].DLAST_SGA = 0;

DMA0->TCD[2].BITER_ELINKNO = 1;

DMA0->TCD[2].CSR |= DMA_CSR_DREQ_MASK;

...

DMA0->SERQ = 2U;

... (Below inside while loop)

if (Count < Timer)

{

Count++;

}

else

{

Count = 0;

DMA0->SERQ = 2U;

}

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,257 Views
ohiogt
Contributor III

Disregard, I should have set the major loop counter to the number of bytes I needed to transmit.

View solution in original post

0 Kudos
Reply
1 Reply
2,257 Views
ohiogt
Contributor III

Disregard, I should have set the major loop counter to the number of bytes I needed to transmit.

0 Kudos
Reply