UART Array Transfer Using DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART Array Transfer Using DMA

跳至解决方案
2,479 次查看
ohiogt
Contributor III

I'm trying to transfer an array on at fixed intervals over the UART using DMA.  Sample code is below.  The code below only appears to transmit the first byte of the array, with other bytes mixed in sporadically.  I'm not sure if I need the FIFO setup or if I'm missing something else.  Any help would be appreciated.

Shawn

#define UART_BUFFER_LENGTH 9

uint32_t g_UARTBuf[9] = {0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53,0x24494c53};

void InitUART(void)

{

UART0->C2 &= ~(UART_C2_TCIE_MASK | UART_C2_RIE_MASK | UART_C2_ILIE_MASK |

UART_C2_RE_MASK | UART_C2_RWU_MASK | UART_C2_SBK_MASK |

UART_C2_TIE_MASK | UART_C2_TE_MASK);

UART0->BDH &= ~(UART_BDH_LBKDIE_MASK | UART_BDH_RXEDGIE_MASK |

UART_BDH_SBR_MASK);

UART0->BDL &= ~(UART_BDL_SBR_MASK);

UART0->BDL |= UART_BDL_SBR(65U);

UART0->C1 &= ~(UART_C1_LOOPS_MASK | UART_C1_UARTSWAI_MASK | UART_C1_M_MASK |

UART_C1_ILT_MASK | UART_C1_PE_MASK);

UART0->C3 &= ~(UART_C3_TXINV_MASK | UART_C3_ORIE_MASK | UART_C3_NEIE_MASK |

UART_C3_FEIE_MASK | UART_C3_PEIE_MASK);

UART0->C4 &= ~(UART_C4_MAEN1_MASK | UART_C4_MAEN2_MASK | UART_C4_M10_MASK |

UART_C4_BRFA_MASK);

UART0->C4 |= UART_C4_BRFA(3U);

UART0->C5 &= ~(UART_C5_RDMAS_MASK);

UART0->C5 |= UART_C5_TDMAS_MASK;

UART0->MODEM &= ~(UART_MODEM_RXRTSE_MASK | UART_MODEM_TXRTSPOL_MASK |

UART_MODEM_TXRTSE_MASK | UART_MODEM_TXCTSE_MASK);

UART0->IR &= ~(UART_IR_IREN_MASK);

UART0->PFIFO &= ~(UART_PFIFO_TXFE_MASK | UART_PFIFO_TXFIFOSIZE_MASK |

UART_PFIFO_RXFE_MASK | UART_PFIFO_RXFIFOSIZE_MASK);

UART0->CFIFO &= ~(UART_CFIFO_RXOFE_MASK | UART_CFIFO_TXOFE_MASK |

UART_CFIFO_RXUFE_MASK);

UART0->CFIFO |= (UART_CFIFO_TXFLUSH_MASK | UART_CFIFO_RXFLUSH_MASK);

UART0->C7816 &= ~(UART_C7816_ONACK_MASK | UART_C7816_ANACK_MASK |

UART_C7816_INIT_MASK | UART_C7816_TTYPE_MASK | UART_C7816_ISO_7816E_MASK);

UART0->C2 |= (UART_C2_TIE_MASK | UART_C2_TE_MASK);

}

...

DMA0->TCD[2].CSR &= ~(DMA_CSR_BWC_MASK | DMA_CSR_MAJORELINK_MASK |

DMA_CSR_ESG_MASK | DMA_CSR_DREQ_MASK | DMA_CSR_INTHALF_MASK |

DMA_CSR_DONE_MASK | DMA_CSR_INTMAJOR_MASK);

DMA0->TCD[2].CSR |= DMA_CSR_BWC(3U);

DMA0->TCD[2].SADDR = (uint32_t)(&g_UARTBuf[0]);

DMA0->TCD[2].SOFF = 4U;

DMA0->TCD[2].ATTR = 0x0200;

DMA0->TCD[2].NBYTES_MLNO = (4)*(UART_BUFFER_LENGTH);

DMA0->TCD[2].SLAST = (-4)*(UART_BUFFER_LENGTH);;

DMA0->TCD[2].DADDR = (uint32_t)&(UART0->D);

DMA0->TCD[2].DOFF = 0;

DMA0->TCD[2].CITER_ELINKNO = 1;

DMA0->TCD[2].DLAST_SGA = 0;

DMA0->TCD[2].BITER_ELINKNO = 1;

DMA0->TCD[2].CSR |= DMA_CSR_DREQ_MASK;

...

DMA0->SERQ = 2U;

... (Below inside while loop)

if (Count < Timer)

{

Count++;

}

else

{

Count = 0;

DMA0->SERQ = 2U;

}

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,170 次查看
ohiogt
Contributor III

Disregard, I should have set the major loop counter to the number of bytes I needed to transmit.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,171 次查看
ohiogt
Contributor III

Disregard, I should have set the major loop counter to the number of bytes I needed to transmit.

0 项奖励
回复