Two or more sensors Attached with one ADC in TWR-K20D72M can't work simultaneusly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two or more sensors Attached with one ADC in TWR-K20D72M can't work simultaneusly

712件の閲覧回数
bhavinmaru
Contributor III

Hello,

I am working with TWR-K20D72M board as controller and IAREW(IAR Embedded Workbench) software for programming.i download the sample codes from the below link

http://cache.nxp.com/files/32bit/software/KINETIS_72MHz_SRC.zip?fpsp=1&WT_TYPE=Lab%20and%20Test%20So...

in those sample codes they are given the sample codes for ADC interface.on board potentiometer is interfaced with one channel of ADC1 which is ADC1_DM0.please try to solve my below query:

-- Here potentiometer is connected to ADC1 now is it possible to attach more sensors with ADC1(means 2 or 3 sensors simultaneusly on ADC1)?

i also tried by changing ADC selection channel but not works properly.if it is possible then tell me which things i have to change in code.

Thank You

Bhavin

ラベル(1)
0 件の賞賛
返信
1 返信

607件の閲覧回数
bhavinmaru
Contributor III

Is there any update on this? please,help me its an urgent.

Any help in this will be appreciated more

0 件の賞賛
返信