SWD / JTAG adapter without resistors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWD / JTAG adapter without resistors

2,639件の閲覧回数
alexeypanteleyc
Contributor II

Hello!

Could you please advise if the following schematic is recommended for SWD / JTAG adapted for Kinetis MCUs (MKM33):

HardwareDebugConnections - ** Code Red Support Site **  

Or it's better to use another one?

Is it critical to use pull-up and pull-down resistors for SWCLK and SWDIO lines? May the adapter work without them?

Thanks,

Alexey

ラベル(1)
2 返答(返信)

2,209件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alexey,

SWD_CLK is pulled down internally, and SWD_IO is pulled up internally. (You can get this information from MKMXXZXXACXX5RM.)

It isn't critical to use pull-up and pull-down resistors for SWCLK and SWDIO lines. The adapter may work without them.

Debug Port Pin Descriptions.png

The external pull-up shown in some diagrams is for potentially noisy environments, and should be on the order of 10kΩ.

From the Kinetis L Quick Reference User Guide (KLQRUG):

SWD KLQRUG.png

The RESET_b pin should have a 100 nF capacitor close to the MCU for transient protection. It has a weak internal
pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended.(From the Kinetis L Quick Reference User Guide KLQRUG)

RESET_b.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,209件の閲覧回数
alexeyusoltsev
Contributor IV

 Hi Alexey!

As for SWD you no need to add any resistors. At least it worked for me for kv10,mk10,mk22,kv30,kv31,kl27 MCUs. And dont mess with reset-you need reset_b pin to trace to reset of JTAG.

 Best regards and "yda4i",

Alexey.

0 件の賞賛
返信