Transmitter output power configuration in KW36

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Transmitter output power configuration in KW36

3,396 次查看
nsuresh2
Contributor III

Hi XingChang,

As per the KW36 datasheet attached, the transmitter output power can be configured from -30 dBm to +3.5 dBm.

Please let us know the parameter needs to be set to configure the transmitter output power.

Thanks,

Regards,

Naven Suresh 

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

3,115 次查看
xing_chang
NXP Employee
NXP Employee

Hi nsuresh2@visteon.com‌,

Add the following 2 MACROs in the file preinclude.h. The relationship between the set value and the transmit power can be calculated by the following table.

#define mAdvertisingDefaultTxPower_c 20

#define mConnectionDefaultTxPower_c 20

pastedImage_10.png

      0x0028 = 40, so if the setting value is 20, the Tx power is 0.3dBm at 25 ℃.

pastedImage_21.png

pastedImage_22.png

0 项奖励
回复

3,115 次查看
nsuresh2
Contributor III

Hi XingChang‌,

Thanks for your quick response.

So as mentioned above both the macros are enabled and set to the default value of 20

When we measure the power it shows -2.39 dBm at room temperature, but as per the above table it should be 0.3 dBm

What could be the reason for this? Any other parameters that need to be looked into this for power deviation?

Thanks!

Regards,

Naven Suresh

0 项奖励
回复

3,115 次查看
xing_chang
NXP Employee
NXP Employee

Hi nsuresh2@visteon.com‌,

The transmit power we measured at the PIN of the chip, if you measure from the SMA, your measurement is reduced by the RF line loss. This is usually around 1dBm, but your loss is a bit big. Please check if the matching network is suitable.

1.jpg

0 项奖励
回复