kI2C_SlaveTransmitAckEvent

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kI2C_SlaveTransmitAckEvent

Jump to solution
1,890 Views
jun1
Contributor V

Hi,
Always I am indebted.

Master-slave communication is being confirmed using “SDK_2.6.0_MKE04Z128xxx4 \ boards \ frdmke06z \ driver_examples \ i2c \ interrupt_b2b_transfer \ slave".

Added kI2C_SlaveTransmitAckEvent to i2c_slave_callback () routine, but does not break there.
When does this event occur?
Is there an API to set ACK / NAK to output manually?

Thank you.

jun.

Labels (1)
0 Kudos
Reply
1 Solution
1,784 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Jun,

Are you using another board to work as master? If so, could you please specify what kind of data you are sending using this peripheral. So that I can try to reproduce this from my end.

Best Regards,

Sabina

View solution in original post

0 Kudos
Reply
2 Replies
1,785 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Jun,

Are you using another board to work as master? If so, could you please specify what kind of data you are sending using this peripheral. So that I can try to reproduce this from my end.

Best Regards,

Sabina

0 Kudos
Reply
1,784 Views
jun1
Contributor V

Thank you very much.
I'll try.

jun

0 Kudos
Reply