Touchscreen and ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Touchscreen and ADC

Jump to solution
2,082 Views
joelesco
Contributor III

Hi !

I use a K70 and I would like to plug a display wich comport a touchscreen. Do i need to use a controller between the touchscreen and the K70 or i can directly plug the touchscreen to ADC pins ?

Thanks a lot !

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,871 Views
LuisCasado
NXP Employee
NXP Employee

Hello Jay,

No, you don't need a dedicated controller, you can use ADC and GPIO. CRTOUCH used in the TWR-LCD-RGB have extra functions like gesture recognitions.

Best Regards,

Luis

View solution in original post

0 Kudos
Reply
2 Replies
1,872 Views
LuisCasado
NXP Employee
NXP Employee

Hello Jay,

No, you don't need a dedicated controller, you can use ADC and GPIO. CRTOUCH used in the TWR-LCD-RGB have extra functions like gesture recognitions.

Best Regards,

Luis

0 Kudos
Reply
1,871 Views
mjbcswitzerland
Specialist V

Hi

There is a guide to using resistive touch screens with ADC/GPIO here: http://www.utasker.com/docs/uTasker/uTaskerTouch.PDF

Regards

Mark

0 Kudos
Reply