The code is generated with CW PE, how to switch the chip quickly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The code is generated with CW PE, how to switch the chip quickly

1,704件の閲覧回数
kabusiji
Contributor I

As shown in the figure:

    福昕截屏20220315093237124.PNG福昕截屏20220315093237124.PNG

I used SKEAZ64MLK4 chips and the code was generated with CW PE.Later, due to the lack of code space, now we need to replace the chip of SKEAZ128MLK4.However, I found that I could only switch the chip of SKEAZ64 through the CPU type of PE. Is there a fast and efficient way to switch? Looking forward for your reply. Thank you!

0 件の賞賛
返信
2 返答(返信)

1,694件の閲覧回数
ErichStyger
Specialist I

You can change the CPU. I wrote about this here:

https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/

 

I hope this helps,

Erich

0 件の賞賛
返信

1,699件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer: Changing the CPU with Processor Expert

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信