The clock mode in KL02

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The clock mode in KL02

1,707 Views
小勇邹
Contributor II

What is the difference between FEI and FBI clock mode in KL02(MKL02Z32CAF4R).

When should I select FEI and when should I select FBI?

If i want to let  the chip work in the internal clock, which mode should I select?

0 Kudos
Reply
3 Replies

1,531 Views
adriancano
NXP Employee
NXP Employee

Hi,

Please refer to the reference manual of the device in the section 21.4.1.1 MCG modes of operation and check the explanation of each module, along with the explanation check the image below that will help you to understand better the information contained there.

fei and fbi.jpg

I hope this can help you to understand the difference between these two modes of operation.

The advantage of using the FLL is that it has a Digitally-controlled oscillator (DCO) and the DCO frequency range is programmable for up to four different frequency ranges. Please refer to the Chapter 21 Multipurpose Clock Generator (MCG) to know more about the FLL and generally about the MCG module.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,531 Views
小勇邹
Contributor II

Thank you very much. What is disadvantage of FEI? When should we select FBI mode?

0 Kudos
Reply

1,531 Views
adriancano
NXP Employee
NXP Employee

Hi,

Since the FBI mode does not use the output frequency from the FLL the frequency options for the Core in FBI mode are the internal clocks frequencies, these are 4 MHz or 32 kHz or any number resulting from the division between 1, 2, 4, 8, 16, 32, 64 or 128 that are the values of the divisor on OUTDIV1 (you can see it in the image I posted before).

In conclusion the FBI mode is a mode that will allow to have a Core clock up to 4 MHz and is used, commonly, when low power modes are used.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply