FRDM K64F: USB MSD with SD Card Bare Metal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM K64F: USB MSD with SD Card Bare Metal

1,467件の閲覧回数
giacomopetrini
Contributor IV

Hi, I found the example in the KSDK/USB floder (dev_msd_disk_frdmk64f120m_bm) that is compiling and working as expected if I select the Ram Disk.

But if I select the SD Card there is acompile error: it can't find the sd.h file.

How can I make it working?

Thank Regards Giacomo

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,233件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Ciao Giacomo,

That function is not enabled in the actual version of SDK (1.0.0), it will be enabled in the next release 1.1 that anyway will be public on December 16th so stay tuned :smileywink:.

Cheers,

Antonio

0 件の賞賛
返信

1,233件の閲覧回数
giacomopetrini
Contributor IV

Ahh ok thanks, at least I have a ETA for next KSDK release.

Regards Giacomo

0 件の賞賛
返信