The I2C driver always returns error "kStatus_I2C_ArbitrationLost"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The I2C driver always returns error "kStatus_I2C_ArbitrationLost"

ソリューションへジャンプ
3,131件の閲覧回数
gauravbanyal
Contributor IV

Hello,

I am trying to communicate with the various slaves I have on the I2C bus on my MKL03Z32 controller. However, the driver always returns error code "kStatus_I2C_ArbitrationLost".

I don't have a clue on why this is happening. The same code was working perfectly on a different schematics using the same uC. Additionally, the uC is the only bus master. So I don't understand why there should be arbitration and why this error is returned.

Please help.

Cheers,

Gaurav.

タグ(1)
0 件の賞賛
返信
1 解決策
2,940件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Gaurav Banyal,

    How many I2C devices you connect in the I2C bus?

   When the problem happens, did you check the I2C bus wave, whether there has some other I2C device influence the I2C wave?

   Please also attached the I2C wave, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,941件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Gaurav Banyal,

    How many I2C devices you connect in the I2C bus?

   When the problem happens, did you check the I2C bus wave, whether there has some other I2C device influence the I2C wave?

   Please also attached the I2C wave, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,940件の閲覧回数
gauravbanyal
Contributor IV

As soon as I connected to the scope to the I2C slave test points, I figured that the slave was not getting powered. HW issue. When that was fixed, it worked like a charm.

0 件の賞賛
返信
2,940件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Gaurav Banyal,

   Good and thank you for your updated information !

  Actually, the I2C is not complicate, next time, if you meet the problem, the first thing is check the I2C bus wave, it will be useful to  locate the root problem.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信